The FLASH diagnostics is organized in the following structure
The analysis reports are listed in this folder.
This folder has the FLASH module diagnostics source code.
This folder has the header file for the FLASH diagnostics source code.